DRV.CLRFAULTS
Description
DRV.CLRFAULTS tries to clear all active faults and warnings on all the axis.
When a fault occurs on an axis, the fault is set and can only be cleared by:
- using AXIS#.CLRFAULTS
- using DRV.CLRFAULTS
- enabling the axis after it has been disabled (either with AXIS#.DIS followed by AXIS#.EN or toggling the hardware enable)
- fieldbuses
A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design that can issue AXIS#.CLRFAULTS
If the DRV.CLRFAULTS succeeds, then AXIS#.FAULTS on all the axes indicate no faults exist. If the fault still exists on an axis after DRV.CLRFAULTS, the fault remains on that axis.
See : Faults and Warning Messages for details regarding the behavior of individual faults.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics